This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/66AK2H14: how to include driver code to our own created application project

Part Number: 66AK2H14

Tool/software: Code Composer Studio

Hi,

I am using 66AK2H14 processor with TI-RTOS/SYS-BIOS using CCSV7 tool.

I created my own application code as required by the client, for that I had to include driver file. So when I include driver file using  "#include", I got fatal error.

c:\ti\pdk_k2hk_4_0_6\packages\ti\drv\gpio\soc\gpio_soc.h:45:30: fatal error: ti/drv/gpio/GPIO.h: No such file or directory
#include <ti/drv/gpio/GPIO.h>

and also how to include ti/drv/gpio/src/GPIO_drv.c- This file contains the GPIO driver interface APIs. These APIs are used for configuration of general purpose I/O instanace. Using that file I have writtern application code.

I request you to tell me the procedure to include driver code to our own created application project as soon as possible.

Thanks and Regards,

Aishwarya Bhat

  • Guru 126455 points
    Aishwarya,

    I can't speak about the entire procedure of how to integrate the driver code into a specific application - the experts at the device forum are usually better equipped to guide you on this task.

    If you want to simply add a source file to your project you can simply follow the details shown at:

    software-dl.ti.com/.../sdto_ccs_build-handbook.html

    I can talk about the specific build error. How did you include the file?

    I see from the PDK package that line 45 of the file <GPIO_soc.h> contains the relative path to the missing GPIO.h file. In other words, it is specified as #include <ti/drv/gpio/GPIO.h>

    This tells me that you need to add the path c:\ti\pdk_k2hk_4_0_6\packages to the compiler include options, so it can properly resolve all relative paths.

    Please give this a try.

    Hope this helps,
    Rafael

    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

  • In reply to desouza:

    Hi,

    Thanks for your reply.

    I have added my files  which I needed. Later I referred example project C:\ti\pdk_k2hk_4_0_6\packages\ti\drv\gpio\test\led_blink\src/main_led_blink.c. It successfully got built without any errors.

    So I included all files, header files, and directories path which are inserted in example project. But when I compiled my project(GPIO_int_app.c) I am getting error for GPIO_board.c file which is also included in already existing example project. Since I have inserted same file from example, I am not able to make out why those errors are coming to my project.

    For your reference I have attached my project and even the screenshot of my project's error. Please help me to solve this error as soon as possible.

    GPIO_int_app.rar

    Thanks and Regards,

    Aishwarya Bhat

  • Guru 126455 points

    In reply to Aishwarya Bhat:

    Hi,

    Thanks for sending the project. I noticed there are a few differences between your project and the example shipped with the SDK (GPIO_LebBlink_K2H_EVM_armTestProject):

    - Some compiler symbols are missing, namely evmK2H and SOC_K2H. (under GNU Complier → Symbols → Define symbols)

    - After inserting these, the project started to show some internal SYSBIOS errors that are described at section 10.6 of the page below:

    http://processors.wiki.ti.com/index.php/Processor_SDK_RTOS_FAQ 

    - Per the description above, I removed the libraries gcc, m, nosys and c from the linker (under GNU Linker → Libraries → Libraries) and matched the paths to the Library Search Path shown in the example project.  

    - I then removed the option -specs=nano.specs from the Linker options (GNU Linker → Miscellaneous → Other flags) and added the option "rdimon.specs" to the Compiler options (GNU Compiler → Miscellaneous → Override built-in specs with... ) - this option adds a few libraries

    - In the same screen I also matched the Assembly source specific flags and Other flags with the example project.

    - I cleaned several include paths and references to source files .

    At this point the project itself failed to build as the main source file does not define the task gpio_test (which you need to define) and other issues related to the migration process per se. In this case, I would strongly suggest you to check with the experts at the device forum.

    The project I modified is shown attached.

    Hope this helps,

    Rafael

    0755.GPIO_int_app.rar


    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

  • In reply to desouza:

    Hi,

       How to contact experts to solve this problem? Can you suggest any one to help me as soon possible.

    Thanks and Regards,

    Aishwarya Bhat

  • Guru 126455 points

    In reply to Aishwarya Bhat:

    Aishwarya,

    I notified another team that may provide additional information.

    Regards,
    Rafael

    When posting, click on the link Insert Code, Attach Files and more... to attach images, files or use nice formatting.

    If my reply answers your question please click on the green button "This resolved my issue".

  • In reply to desouza:

    Hi Rafael
    Thanks for forwarding this to us.

    Aishwarya

    I will ask the software team to help out on this.

    REgards
    Mukul
  • In reply to Aishwarya Bhat:

    Aishwarya,

    I downloaded the project attached by Rafael and was able to get it to build successfully by commenting out the line Program.global.echo = Task.create("&gpio_test", task0Params); in GPIO_int_app.cfg (since it appears you are not using this task).

    I hope this helps. Please let us know if you run into any other issues.

    Best,
    Sahin

    Sahin Okur
    Applications Engineer

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.