• TI Thinks Resolved

CCS/TMS320C6657: SRIO lane speed issues (TI to TI, TI to Zynq comm)

Part Number: TMS320C6657

Tool/software: Code Composer Studio

Hi TI experts,

We are configuring a TI DSP (c6657) board to talk to another of c6657 board, and also a Xilinx Zynq board.  The set up includes all three boards & a Vadatech UTC 2002 switch in a MicroTCA Chassis. Upon configuring the TI DSP board that we are using as our master for different numbers of lanes (1 or 4 lanes), we do not see a linear change in speeds (very little change in speeds at all, about 10%). We have also noticed that the RIO_PLM_SP_PATH_CTL register shows does show Configuration 4 mode 0 (when attempting single lane) or Configuration 4 mode 4 (while in four lanes). We have compared our results to the "Throughput Performance Guide for KeyStone II Devices" and see that our speed changes should be changing proportionally when changing from 1 lane to 4 lane communications.  Ours are most certainly not, but we have done everything in our ability to figure out why, but to no avail.

We also see very different speeds when performing NREADs from TI(A) to TI(B) and from the Zynq to TI(B), which we believe is to be expected because the "TI has eight LSU register sets, allowing for eight outstanding requests for all transaction types that require a response," while the Zynq needs to wait after each packet for the response.  Is this what should be expected?  We are seeking assistance in finding the root of this issue. Thanks for your time.


Bandwidths:

4 lane NREAD TI(A) to TI(B): 235MB/s

1 lane NREAD TI(A) to TI(B): 226MB/s

4 lane NREAD TI(A) to Zynq: 235MB/s

4 lane NREAD Zynq to TI(B): 19MB/s

1 lane NREAD Zynq to TI(B): 19MB/s

  • In reply to Josh Cherry:

    Josh,

    The more important one Serders register is SRIO_SERDES_CFGPLL SerDes (0x02620360), see the Serdes register list in SPRUGW1B table 3-2.

    SERDES MACRO REGISTERS
    0x02620154 SRIO_SERDES_STS SerDes Macro Status Register
    0x02620360 SRIO_SERDES_CFGPLL SerDes Macro Configuration Register

    SERDES RECEIVE/TRANSMIT CHANNEL CONFIGURATION REGISTERS
    0x02620364 SRIO_SERDES_CFGRX0 SerDes Receive Channel Configuration Register
    0x02620368 SRIO_SERDES_CFGTX0 SerDes Transmit Channel Configuration Register
    0x0262036C SRIO_SERDES_CFGRX1 SerDes Receive Channel Configuration Register
    0x02620370 SRIO_SERDES_CFGTX1 SerDes Transmit Channel Configuration Register
    0x02620374 SRIO_SERDES_CFGRX2 SerDes Receive Channel Configuration Register
    0x02620378 SRIO_SERDES_CFGTX2 SerDes Transmit Channel Configuration Register
    0x0262037C SRIO_SERDES_CFGRX3 SerDes Receive Channel Configuration Register
    0x02620380 SRIO_SERDES_CFGTX3 SerDes Transmit Channel Configuration Register

    Regards,
    Garrett
  • In reply to Garrett Ding:

    Garrett,

    The values pulled from the registers (directly after setup & configuring the routing table) are below:
    0x02620154: 0x08112245
    0x02620360: 0x00000229
    0x02620364: 0x00440495
    0x02620368: 0x00180795
    0x0262036C: 0x00440495
    0x02620370: 0x00180795
    0x02620374: 0x00440495
    0x02620378: 0x00180795
    0x0262037C: 0x00440495
    0x02620380: 0x00180795

    Thanks again for your support,
    Josh
  • In reply to Josh Cherry:

    Josh,

    So from the serdes registers, we know the MPY = 5, and operating rate is half (01b), what is your SRIO reference clock frequency and did you refer to the Table 3-7 Frequency Range versus MPY Value in UG to check if the serders are configured properly in all test cases?

    Regards,
    Garrett
  • In reply to Garrett Ding:

    Garrett,

    Our ref clk is 250MHz, and we did verify that the Data Rate was 2.5 Gbps, as we expected. This value shouldn't change as we configure for different lane combinations, should it?

    Again, we greatly appreciate the help.

    Thanks,
    Josh
  • In reply to Josh Cherry:

    Josh,

    Yes, the data rate (2.5Gbps) should be consistent for different lane combinations.

    >>We are using a modified version of the device_srio_loopback.c file found under the pdk_c665x_2_0_7 directory to initialize our SRIO device.

    What are the modification you have done? Have you tried to measure the throughput with the breakout card setup like described in the thread e2e.ti.com/.../436245
    for the test case -
    4 lane NREAD TI(A) to TI(B): 235MB/s
    1 lane NREAD TI(A) to TI(B): 226MB/s

    Did you find out the difference of Serdes and SRIO register values in the two test cases with your setup?

    Regards,
    Garrett
  • In reply to Garrett Ding:

    We have continued to have issues, but now think it may be easier to utilize code that TI has rendered. Do you have the code associated with the results from the throughput performance document that we could try to use? I apologize for the delayed response, we have had a busy week.

    Thanks again,
    Josh
  • In reply to Josh Cherry:

    (Edited)

    Josh,

    The code associated with the throughput performance document should be the old MCSDK - software-dl.ti.com/.../index_FDS.html for keystone 2 device, and  for keystone I e.g. C6657 device, which are no longer maintained, and we have moved to Processor SDK as you may know.

    Regards,
    Garrett

  • In reply to Garrett Ding:

    Garrett,

    We utilized the "Tput" code in SRIO from the BIOS-MCSDK 02 01 02 above. We ran the code in three different configurations, but found the same results. We are still using the C6657 board. What might the issue be?

    4x Lane, 5 GBaud
    Bytes |  Thruput
    4         |   83.33
    8         |  166.67
    16      |   333.33
    32      |  666.67

    1x Lane, 5 GBaud
    Bytes |  Thruput
    4         |   83.33
    8         |  166.67
    16      |   333.33 
    32      |  666.67 

    1x Lane, 3.125 GBaud
    Bytes |  Thruput
    4         |   83.33
    8         |  166.67
    16      |   333.33 
    32      |  666.67 

    Thanks,
    Josh