This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DDR3 on 6678 EVM

Is there a BOM available somewhere for the 6678 EVM?  In particular what's the part number for the DDR3?

---------------------------------------------------------------------------------------------------------
http://processors.wiki.ti.com/index.php/User:BradGriffis
--------------------------------------------------------------------------------------------------------- 

  • The BOM is not yet available for the C6678 EVM.  The C6678 EVM is designed to support a full 72-bit memory topology (includes ECC bits) using JEDEC-compliant DRAM devices.  It is implemented using x16 DRAM devices for the data and either a x16 or a x8 DRAM device for the ECC memory.  Initial EVMs will be populated with 1Gb or 2Gb DRAMs from Samsung, Micron or Elpida.  Possible part numbers are SAMSUNG K4B2G1646C-HCH9 or Elpida EDJ1116BBSE-DJ-F.

     

    Regards,
    Tom Johnson
    Hardware Applications Engineer
    Embedded Processors

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.