This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

C667x boot via DM3730

How do I boot the C667x multi-core DSPs from the DM3730?  The SPRUGY5 suggests to use the HyperLink boot mode. 
 1. How do I map the HyperLink interface to the DM3730?  
 2. Are the drivers for the HyperLink interface on the C667x and on the DM3730 available?
 3. Are the drivers TSIP, SPI, SRIO, and EMIF16 for the C667x available?
Regards,
Sy 

  • Sy Tran

    How do I boot the C667x multi-core DSPs from the DM3730?  The SPRUGY5 suggests to use the HyperLink boot mode. 
     1. How do I map the HyperLink interface to the DM3730?  
     2. Are the drivers for the HyperLink interface on the C667x and on the DM3730 available?

    There is no HyperLink interface on the DM3730, so this option is not valid.  The datasheet for the C667x indicates a SPI or I2C boot mode is supported.  These interfaces are on the DM3730.

    Brandon

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.