I want to program the "hello word " demo with nor flash via I2C boot , but when I Program "IBL Configuration"table wtih EEPROM, I has the problem:
steps for Programing "IBL Configuration":
(a) Make sure that the boot mode dip switch is set to no boot/EMIF16
boot mode on the EVM (please refer to the EVM technical reference manual
on how to set the boot mode dip switches.
(b) Open CCSv5 and launch the evmc66xx emulator target configuration and connect to core 0.
(c) Load the program i2cparam_c6678_le.out to CCS.
(d) Run the program and a message "Run the GEL for the device to be configured,
press return to program the I2C" will be printed on the CCS console.
(e) Load i2cConfig.gel (in CCSv5 Tools->GEL Files, right click mouse in GEL Files
window and select "Load GEL"
(f) Run the GEL script "EVM c6678 IBL"->setConfig_c6678_main, this will set the
default boot parameters for booting application images from NOR, NAND and
Ethernet.
(g) Now press "Enter" in the CCS console window, and the program will write the
boot parameter table to the EEPROM. On success the message "I2c table write complete"
will be printed on the CCS console
IN step (d), the ccs output this :" cont find "memst.c" file,then I locate the file,and goon,
IN step (g), the CCS run all the time without an end,maybe DSP is error
So, as a result , I cann't boot the demo from noe flash via I2C ,can you help me?
Thanks!