Hi,
I wonder if the transcode demo packaged with the mcsdk-video must run in ROM Ethernet Boot mode?
Does it work if I set the boot mode to I2C boot.
Thank you!
Sunzhao
Hi Sunzhao,
The transcode example does not have to run in ROM Ethernet Boot mode. It can run in I2C boot mode, and also the other boot modes listed in http://processors.wiki.ti.com/index.php/TMDXEVM6678L_EVM_Hardware_Setup#Boot_Mode_Dip_Switch_Settings.
For running the transcode example, please find more details from another post: http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/177287.aspx.
Thanks,
Hongmei