Hi,
I run nwal test (nwal_c66x_1_0_0_1)program packaged with mcsdk_video_2_0_0_10 in C6678 with CCSv5.
But it got error below. "nwal_addConn returned Error Code -3" seems error from PA. Please help me check how
to resolve this issue. Thank you!
[C66xx_0] CORE: 0 Global and Local Network initialization Successful CORE 0: Adding MAC entry MAC Open sent with trans_id: 0CPSW ALE table updated for the destination MAC address CORE: 0 Adding IP entry - SRC=[1, 2, 3, 4] IP Open sent with trans_id: 0CORE: 0[C66xx_0] Adding UDP entry CORE: 0 Adding Port config, port: 0x555 CORE: 0 ERROR: nwal_addConn returned Error Code -3 [C66xx_0] CORE: 0 Global and Local Network initialization Successful CORE 0: Adding MAC entry MAC Open sent with trans_id: 0CPSW ALE table updated for the destination MAC address CORE: 0 Adding IP entry - SRC=[1, 2, 3, 4] IP Open sent with trans_id: 0CORE: 0[C66xx_0] Adding UDP entry CORE: 0 Adding Port config, port: 0x555 CORE: 0 ERROR: nwal_addConn returned Error Code -3
Sunzhao
Hi Sunzhao,
Which platform are you using to run the test program? Single C6678 or the one with 4 C6678?
Thanks,
Hongmei
Hi Hongmei,
The platform here is DSPC8681 too. I Just want to know what is the reason to cause this
error and how to resolve it? Thank you!
BTW. Will you please help me check these more issues below:
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/180645.aspx
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/179652.aspx
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/179676.aspx
Thanks a lot!
We verified the NWAL test program on DSPC8681 with the procedure below:
Can you please let us know the version of tools you used for compiling the NWAL test program?
The set of tools shall be the same as those used in MCSDK Video 2.0:
xdctools_3_22_04_46
pdk_C6678_1_0_0_17
ipc_1_24_00_16
bios_6_32_05_54