I was wondering if there was a document/utility or if I could get some get some help decoding the EABI file format for bootloading. I've used the hex6x utility to successfully make a boot file, however, I'm in the process of making a secondary bootloader to load out of a large I2C device (3/4 byte addressing), and the one issue I currently have are the sections of code we need to prefill w/ 0x00.
I've used the ofd6x utility to successfully create a xml file, however I'm having an issue trying to find where the pre-fill values are. Is there a document out there that describes the xml output (like the http://www.ti.com/lit/an/spraa64/spraa64.pdf for COFF files), for the EABI output?