Hi,
I have c6678, in the GbE Switch Subsystem data sheet in page 70 there is a table with offset address of the GbE registers.
I can't find the GbE Switch Subsystem address in the Memory Map Summary in c6678 data manual.
Thanks,
Aviv
Hi Aviv,
Please check sprugz6 - NETCP User Guide page 16 paragraph 2.2 - Memory Map,
BR,
HR
The address range is defined in the Memory Map of the Data Manual (Table 2-2)
02000000 020FFFFF 0 02000000 0 020FFFFF 1M Network Coprocessor (Packet Accelerator, Gigabit EthernetSwitch Subsystem and Security Accelerator)
The offset base addresses to the specific modules are defined in the UG as mentioned by HRi. Use these with modules register offset values for the register location.
Best Regards,
Chad
------------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.