Hi everyone,
There are two C6678 DSPs ,whose ethernet interface are connected directly, on my board.
My goal is that C6678_A sends some data and C6678_B receives them correctly. I found an example project
under pdk_C6678_1_0_0_17\ packages \ ti \ drv \ exampleProjects \ PA_emacExample_exampleProject.
The remark in the example codes says that the packets sent by the application are sent on the wire and
since the destination MAC on the packet is the Ethernet switch MAC address,the packets are received by
simulator and passed back up to the example application for processing.
In my case,the packets sent by the C6678_A should be received by C6678_B. So I must set C6678_B's
IP address, MAC address and port number in codes running in C6678_A. Here are my questions.
1. How to allocate an IP address,MAC address and port number for C6678_B?
2. What function should be performed by the program running in C6678_B?
3. Why this project reffered above can't be run in single steps?
I am looking forward to your reply. Thank you very much.
Best Regards,
Nuoxi