I boot my C6678 by SPI + Nor Flash.
I have only one Project , so only one .out file , translate it to .dat file and write it to flash .
When the C6678 boot , the bootloader will download the image to only core0 or all of the 8 cores automatic ?
The CMD file of My Project use the logic Address , so all of the Cores have the same memory map , so i dont think i need the MAD .