Hi,
I'm trying to use the Memory Proteciton Unit of the C6678 to deny accesses to the CFG space of the slave devices.
As to my understanding of the SPRUGW5 document I have to clear all the AID fields to deny the accesses. (page 15). But when set all AID field to 0 nothing happens every access is granted.
So next I cleared the complete MPPA register (AID and SR, SX, SW, ...) to '0'. But the result was the same: every access is granted.
Only when I set the AID-bit to '1' (for the corresponding master) and set access mode register bits (SR, SW, ...) to '0', the access is succesfully denied.
Can someone please explain me the meaning of the AID-Bit fields?
Thanks.