Hello,
I am using CCS 5.2 along with MCSDK 2_00_09_21 and NDK 2_21_00_32 on a EVM C6670. I am trying to understand the helloWorld_ndk example and during the init phase the following msgs are printed on the console:
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7
[C66xx_0] Registration of the EMAC Successful, waiting for link up ..
Now, when I go through the code I couldn't find the fxn which does the init of the PASS and the EMAC and then prints out the above msgs! It is done after NC_Netstart() is executed and before jumping into NetworkOpen() callack fxn.
Thx in advance!
BR
Burak