Note: This is with K2 EVM 1.1
I've been using a version of the keystone U-Boot I grabbed around June 2013 (around the time of MCSDK mcsdk_linux_3_00_00_11) along with the ./images from a newer version of MCSDK (mcsdk_linux_3_00_03_15) and it has been starting the linux kernel just fine.
I decided to upgrade my version of U-boot and now the booting will not get past Starting kernel ...
As a quick test if I flash the .gph that came with mcsdk_linux_3_00_03_15, standup a tftp server and run the default u-boot boot of ramfs, it feezes at Starting kernel ...
If I move back to my mcsdk_linux_3_00_00_11 directory, load the .gph that came with it, and do the same thing, the arago-console image boots just fine.
Is this somehow related to my EVM version?