Hello,
I would like to confirm more detail about MSMC MPAX register access.
Question
- Is the following operation 2) allowable on 66AK2H?
Because, it might be correspond the following restriction on TRM(spruhj6: P25).
Best regards, RY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It looks to me from the diagram you're simply changing the address mapping configuration, correct? As long as you follow the guidelines and restrictions as you've pointed out, this is perfectly valid.
I general this is done as a one time upfront change, if you're planning on changing it dynamically, you'll need to put SW in place to make sure that no system ports access the SES Interface frome the same PrivID, but it would be allowable.
Best Regards,
Chad
Chad-san,
Thank you for your prompt response.
Your understanding is almost correct, but I would like to compensate a little bit.
Chad Courtney said:you'll need to put SW in place to make sure that no system ports access the SES Interface frome the same PrivID, but it would be allowable.
During changing segment 1, other SoC master(EDMA etc..) will always access segment 0 from the same PrivID.
Is it allowable? (Note that no access on segment 1.)
Best regards, RY
If the access is ongoing, you would need to stop traffic from that PrivID that is using the SES Interface when you're modifying the MPAX registers. You could halt accesses, make MPAX configuration changes and start accesses again.
Note that doing such you'll need to do manual cache coherence operation if the data space is cached.
Best Regards,
Chad
Chad-san,
Thank you so much for your support.
To satisfy the MPAX configuration rule, I am considering other method.
May I confirm if the following situation is allowed or not?
I would like to change MPAX register dynamically.
From previous your answer, I understood:
Modifying the MPAX registers during other SoC master access to the segment is NOT allowed.
Instead, I am considering to use sRIO (Direct I/O) to access both data segment and MPAX registers. (There is no other SoC master access.)
From the macro point of view, it means only one access to SES Interface at a moment.
It can be satisfy the MPAX configuration rule. Is that right?
For detail, I would like to send you pdf file.
It must treat as confidential. Do you have any method to send it to you?
Best regards, RY
As long as it's not violating the other requirements "It is required that updates to memory-mapped registers are not made while accesses are being made through any of the system ports that utilize the registers being written to." then it's valid. The SRIO isn't violating this, but make sure there's no other traffic that would be violating it as you're changing the MPAX configuration.
Best Regards,
Chad
Chad-san,
I am sorry. I had misunderstanding about previous question.
May I have once more confirmation?
RY9983 said:From the macro point of view, it means only one access to SES Interface at a moment.
It can be satisfy the MPAX configuration rule. Is that right?
From the macro point of view, there are two types of access.
access a) sRIO to DDR3A via MSMC SES Interface.
access b) sRIO to MPAX registers via MSMC SMS Interface.
But, sRIO issues only one transaction either access a) or b) at a moment.
It can be satisfy the MPAX configuration rule. Is that right?
Best regards, RY
Ry,
Assuming that the MPAX registers being modified in b.) are for the control of addressing used in a.) then this would be violating the requirements.
Best Regards,
Chad
Chad-san,
Thank you for your reply.
Chad Courtney said:Assuming that the MPAX registers being modified in b.) are for the control of addressing used in a.) then this would be violating the requirements.
I understand.
May I have confirmation along my case.
In my considering case, there are two data streaming (streaming A and B).
I am considering like following:
streaming A :
a. Data transfer from sRIO to DDR3(area A)
b. After that, MPAX addressing is modified to area C from area A.
streaming B :
c. Data transfer from sRIO to DDR3(area B)
d. After that, MPAX addressing is modified to area D from area B.
During "a" of streaming A, "d" might be occured. (During "a" of streaming A, "b" has never been occured.)
Can It be satisfied the MPAX configuration rule?
And, I am asking to local FAE support to send you confidential pdf file.
Best regards, RY
RY,
You could potentially get into issues if just using NWrite packets since the memory writes will be different paths than the register writes. What I mean is that if the write transactions are loaded into the LSU back-to-back, SRIO will fire the transactions as fast as possible.
So if the write to DDR3 is sent, followed immediately by the write to the MPAX register, it is possible the register write may pass the other transactions because of the SoC internal paths and/or any stalls on DDR3. The best thing to ensure that the writes completed before sending the MPAX register write is to either use NWRITE_R for the last DDR3 write transaction, or use NWRITE followed by a DOORBELLL packet. This will ensure that the NWRITE_R or DOORBELL response packet is received before the LSU will send the MPAX register write packet.
Best Regards,
Chad
Chad-san,
Thank you so much!
Your suggestions are very helpful for us.
In conclusion, there are two method you said:
Method A) use NWRITE_R for the last DDR3 write transaction
Method B) use NWRITE followed by a DOORBELLL packet
In our system, I would like to use sRIO as 5Gbps x2lane x2port mode.
Each ports are connected to FPGA, and both sRIO ports stream data to 66AK2H from FPGA.
Q1) In this case, can I use "Method B"?
Q2) When I use "Method A", can you imagine the actual throughput?
About Mehtod B, I am considering to following process.
Step 1) SWRITE: Data streaming
Step 2) DOORBELL: Wait for previous SWRITE transaction
Step 3) NWRITE_R: Change MPAX register
Step 4) SWRITE: Consecutive data streaming
Best regards, RY
RY,
That should be fine assuming the 2nd SRIO port is not transmitting to the same data space (i.e. it cannot be an outstanding transaction on the SES port to the space that's being reconfigured.)
Best Regards,
Chad
RY,
I think that's really going to be system dependent. If moving large amounts of data in between changes, then the impact should be minimal and approaching the throughput numbers documented in the Throughput Application note.
Best Regards,
Chad
Chad-san,
Thank you for your reply.
"the Throughput Application note" is sprabk5a. Right?
http://www.ti.com/lit/an/sprabk5a/sprabk5a.pdf
Do you have throughput document for KeystoneII?
Or, could you let me know its release schedule?
Best regards, RY
RY,
Yes, that's the Throughput App Note, I referred to. There's not a separate one for Keystone II devices. The SRIO Throughput performance numbers are going to be the same.
Best Regards,
Chad
Chad-san,
Thank you for your seamless support !
Chad Courtney said:Yes, that's the Throughput App Note, I referred to. There's not a separate one for Keystone II devices. The SRIO Throughput performance numbers are going to be the same.
Although there is NWRITE performance in sprabk5a, NWRITE_R performance does not exist.
Do you have NWRITE_R performance ?
Best regards, RY
NWRITE_R is going to have similar performance to that of NREAD. Please keep in mind that it's only needed to perform the NWRITE_R on the last transaction prior to performing the writes to the MPAX registers.
Best Regards,
Chad
Hello,
I am evaluating the changing of MSMC segment by sRIO direct I/O transfer.
In our exam, I am using DualEVM_BOC board to connect both K2HEVM and 6678EVM.
And, sRIO transfer is succeeded from C6678 to DDR3A/sRIO cfg area.
But, when I perform NWRITE transfer to MSMC config registers area(0x0BC00000) by C6678, "RX IO Access" error is happened in K2H side ERR_DET(0x0290C008) register.
I am using PDK example:
- K2HEVM side:
C:\ti\pdk_keystone2_3_00_04_18\packages\exampleProjects\SRIO_TputBenchmarkingK2KC66TestProject
- C6678EVM side:
C:\ti\pdk_C6678_1_1_2_6\packages\ti\drv\exampleProjects\SRIO_TputBenchmarkingTestProject
Question)
Do you have any idea to avoid this error?
Do I have to set sRIO as supervisor mode?
If you need more information, please let me know.
Best regards, RY
Yes, the RX I/O Access error happens when SRIO tries to access a memory address that is memory protected/restricted. Check to make sure the address is valid and a global address, and also try the source ID that is set in the supervisor register.
Regards,
Travis
Travis-san,
Thank you for your reply.
- The sRIO direct-IO mode can access to MPAX registers. Is that right?
- To become the supervisor mode, I configured following register:
SUPRVSR_ID (0x02900E4C) = Transfer ID (0x2 in my case)
I could see the 0x2 in ID_CAPT (0x0290C018) register.
Do I have to configure other registers?
Best regards, RY
SRIO should be able to access the MPAX SES/SMS registers since they are memory mapped. I'm not sure of the privilege requirements, but supervisor should definitely work.
Your understanding of the SUPRVSR_ID register is correct. So as long as the packet's SRCID = the value stored in this register, the internal VBUS transaction will occur at supervisor priveleges. No other register configurations are needed.
Regards,
Travis