Our customer designs the custom C6657 boards which can use with a PC environment via PCIe.
The power supply of the C6657 board is not supplied from a PC module. Separate power supplies are used for the C6657 board and the PC module each.
Only one side of those power supplies can be supplied, and then only one side of a PCIe lane can be driven. Those conditions may give the damage to the devices.
If the C6657 board is powered-up and operates before the PC module is powered-up, can it avoid the damage to the devices that the power domain of C6657 PCIe is disabled by PSC?
Can the PC module be powered-up and operate before the C6657 board is powered-up?
Best regards,
Daisuke