I want to run H265 demo program of video mcsdk.
but It seems that the demo program in the video mcsdk is for the DSPC-8681 or 8682.
what should i do to run H265 demo program on the evm6678l?
Best Regards,
kwangjoo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to run H265 demo program of video mcsdk.
but It seems that the demo program in the video mcsdk is for the DSPC-8681 or 8682.
what should i do to run H265 demo program on the evm6678l?
Best Regards,
kwangjoo
Hi Rajasekaran K,
sorry, the description of my testing environment was lacking.
we are using the evm6678l with the "AMC TO PCIe adapter card" and this have been pluged into the PCI socket on motherboard. (network don't use)
and when running PCIe_H265enc_demo program by MCSDK_VIDEO_2.x_Getting_Started_PCIe_Demo_Guide, demo program stopped after parameter setting.
and I want to know that the PCIe_H265enc_demo can run on the evm6678l.
Best regards,
Kwangjoo
Hi Kwangjoo, could you please send us the scripts you are trying?, how many cores are you using?
thank you,
Paula
Hi paula,
Please see the attached file.
and we are using 8 core.
Best Regards,
Kwangjoo
Hi Kwangjoo, from the scripts it seems you are using only core0 (-t "0") you can use instead
-t "0 1 2 3 4 5 6 7"
Also, I haven't tried --iter for file2file enconding scripts, could you please take out for a quick test?
You could face another issues due to memory mapping. Currently HEVC assumes a Quad or Octal shannon boards which has the double of DDR than a Shannon EVM. But you can give a try and let us know.
thank you,
Paula
Hi Kwangjoo,
I want to inform you that our latest MCSDK Video 2.2.0.39 will include the option to run HEVC on a single Shannon EVM. This drop will be soon published on the web. I will let you knwo when it is release so you can try it.
thank you,
Paula
Hi Kwangjoo, please check below link for MCSDK video drop 39
http://software-dl.ti.com/sdoemb/sdoemb_public_sw/mcsdk_video/02_02_00_39/index_FDS.html
You can now test out-of-box our HEVC on a single Shannon EVM. Please let us know if you have any question.
Thank you,
Paula