dear sir:
i'm developing a system based on c6678. In order to simplify the design, the nor flash on the evm board from
advantech is removed. Now I doubt if the system can boot just by i2c eeprom and nand flash?
I read some article in this forum which point out that the codes in i2c eeprom do some initialization, then the dsp
can access the nand and boot flow jumps to the nand code, then boot can be completed, can it really work?
If I want to run the linux, is this architecture OK?
thanks!