I need to transmit data via SRIO and i need to translate the address from Local L2 (0x00800000 -> 0x0087FFFF) to Absolute (0x10800000 -> 0x1087FFFF for core 0 and so on) for each core
Since this part of the code will be identical in all the 8 cores, there is a register that allows me to identify the core on which the program is running?
Thanks