Hello,
Can I have IBIS model of 66AK2H12/06 ?
I have refered TCI6636K2H product page, and I found IBIS.
Is it same as 66AK2H12/06?
sprm588.zip
http://www.ti.com/product/tci6636k2h
Best regards, RY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can I have IBIS model of 66AK2H12/06 ?
I have refered TCI6636K2H product page, and I found IBIS.
Is it same as 66AK2H12/06?
sprm588.zip
http://www.ti.com/product/tci6636k2h
Best regards, RY
Rajasekaran-san,
Thank you for your support !!
I got IBIS model from local support.
Although I would like to use peripherals of PCIe, SRIO, SGMII, USB, DDR3, there is no SerDes simulation in IBIS model.
But, I noticed Notes in .ibs file:
| ___________________________________________________________
|
| **For SerDes simulations use Texas Instruments IBIS AMI models**
| ------------------------------------------------------------
a) What is IBIS AMI models? How can I use it?
b) And, only DDR3 simulation model exist in .ibs file. Can I use it?
Because DDR3 is generally SerDes (It is not LVCMOS), I need to confirm if I have to use the IBIS AMI models or not.
I need simulation model until May 7th about a).
Since I have already started simulation of DDR3, I need information as soon as possible about b).
Best regards, RY
RY-san,
The IBIS model that you have should be sufficient for modeling DDR3. DDR3 is not a Serdes interface. To model the serdes interfaces you will need a simulation package that accepts AMI models as part of the IBIS input. These models are not available on TI.com and you must have a signed NDA agreement to receive them. Please contact you local FAE to start the process to get the AMI models if they are needed.
Regards, Bill