Question from the customer:
We have traditionally run the TMS320C6678 is little Endian mode. I see that the processor has an Endian configuration. Can it be configured to run in Big Endian? Do you have customers running it in that mode? I also noticed that the example CCS projects distributed by TI are in LE. Do you have example project for BE? Are there any know issues running it in BE? Is the processor "native" to either?
The driving force for us is that the PCIe and the other processors in the system are natively BE and we were wondering if running the TI processor in BE as well, would make things easier.