Hi!
I'm working with my custom board with C6678 DSP. I try to read from on-board I2C EEPROM. I write I2C chip address and I2C memory address as master-transmitter, and then I want to set RESTART condition with READ bit. But after I write the RESTART condition with READ bit I read RSFULL bit set in I2C ICSTR register. Is it an error condition? Or is it the expected condition as it says in sprugv3 Table 2-1?