Hi,
I have some questions regarding Keystone2 architecture.
Now, I see two technical documents. One is MSMC User Guide. Other one is 66AK2H14 data manual.
The following are my questions.
1)According to the MSMC User Guide, MSMC has only one slave port (ARM CorePac Coherent Slave Port) for ARM CorePac. Also the port to DDR3 memory (MSMC EMIF Master Port) is only one. I think that these facts mean multiple ARM Cores can't access to the address of DDR3 memory access in same time even though the address is different.
Is my understanding right?
2) As to my understanding, the route from ARM CorePac to DDR3 is the following.
ARM CorePac --> MSMC --> (MSMC EMIF Master Prot) --> DDR3 EMIF ---> DDR3 memory
Are there any routes execept for the above? If there is, please let me know the route.
I appreciate your quick reply.
Best regards,
Michi