Hello All,
I was wondering if anyone has thought about this - probably so - but is it possible (I think so) - to use the RapidIO Interface on the EVMK2H as a CSI-2 camera interface?
Probably an adapter board would have to be made - but can the signaling be adapted to get data from a CSI-2 based camera? And/or - could a CSI-2 TX 'emulator' be coded up to tx CSI-2 signals?
Just thinking out loud a bit here - but since CSI-2 is (Sub)LVDS, it would appear this is a possibility and something that could be interesting to work on.
Thanks In Advance,
johnw