Hi Champs,
According to C6654/55/57 Errata (SPRZ381A), a workaround of advisory 3 mentions DDR3_CONFIG_REG_23 register as follows.
o C6654/55/57 Silicon Revision 1.0 Silicon Errata [SPRZ381A]
(http://www.ti.com/lit/pdf/sprz381)
- Page 12
Advisory 3 DDR3 Automatic Leveling Issue
Workaround:
...To do this, leave the read data eye training enabled
(leave bit 9 in DDR3_CONFIG_REG_23 = 0),
But the register is not available for C665x as below.
o KeyStone DDR3 Memory Controller U/G [SPRUGV8D]
(http://www.ti.com/lit/pdf/sprugv8)
- Page 58
Table 4-2 DDR3 PHY Leveling Registers (See device datasheet for base address)
(Part 1 of 2)
Offset : 460h
Acronym: DDR3_CONFIG_23 (NA for TCI6614 and C665x devices)
So, I think the errata info is not the latest one. Can I get the latest errata?
Regards,
j-breeze