I'd like to bring up a topic from last year which couldn't be solved then:
I would like to exchange high-speed serial data data between the EVMK2H and a Xilinx Series 7 evaluation board (e.g. VC707 or KC705), preferably via the 4 Serial Rapid IO lanes located on the AMC B+ connector.
For last-generation EVM boards there is a AMC-to-PCIe adapter board (TMDXEVMPCI) available which unfortunately doesn't fit to the EVMK2H board. The best solution would be some kind of adapter AMC <--> FMC to directly connect the DSP and the FPGA evaluation boards with each other.
I wonder how other people manage to exchange data with this EVM without buying additional carrier boards and a backplane or rack?
Suggestions would be greatly appreciated.
Chris