we use the c6657 spi boot ,after we change the switch to the spi boot mode ,we use the oscilloscope to observe ,we found that the dsp send the same command(0x03000000 which is the read command plus the address),then the flash send to the dsp the same data (1651, the first data in the .dat file) ,I want to know why not the address increase ,does the RBL run into a endless loop? if it run into the endless loop ,why?