Hi
I have two DSPC8682 boards (total 128 cores), and I tried to run H265 Encode demo but got a stuck at processing.
Does H265 encoder not support multi-board?
Environment:
Ubuntu 12.04
Memory: 16GB DDR3
DSPC8682 *2
Desktop Linux SDK 1.0.1.0
MCSDK Video 2.2.0.38/39/41
Used command:
./reset_dsp.sh 1250
./dnld_dsp.sh 16
# Use 32 cores with core #64 as master which is the first core on the 2nd board.
$MCSDK_VIDEO_HOSTBIN_DIR/demo_c667x
--dsp-image=$MCSDK_VIDEO_DSPIMAGE_DIR/sv04.out -v --channel="H265
Encode" -a HEVCENC -f $CLIP_CONFIG -c $CODEC_PARAMS -t "64 65 66 67
68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93
94 95" --width=1920 --height=1080