Hi,
I am looking for a simple example for toggling GPIO LEDS on my 6657 EVM.
Which GPIO connected to each LED ?
I don't want to use platform.h functions..
Thanks,
Ivgeni.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am looking for a simple example for toggling GPIO LEDS on my 6657 EVM.
Which GPIO connected to each LED ?
I don't want to use platform.h functions..
Thanks,
Ivgeni.
Hi,
This example turns on EVM board leds.
I need to turn on specific GPIO leds :
How can I access them and turn them on >?
Hi,
As per C6657 EVM schematics, the above specified pins are used for TIMER OUT & UART.
You shall use the GPIO0-15 for your case.
Please refer evmc665x_gpio.c & evmc665x_gpio.h source under ..\ti\pdk_C6657_1_1_2_6\packages\ti\platform\evmc6657l\platform_lib for usage.
Thank you.
Hi Ivgeni,
No, You can use unused GPIO pins for your testing. Please refer C6657 EVM schematics.
Thanks,
Hi,
I want to turn on GPIO18 GPIO19 GPIO20 GPIO21.
can I use this commands ?
gpioSetOutput(18);gpioSetOutput(19);gpioSetOutput(20);gpioSetOutput(21);
Should I write any other commands ?
Thanks,
Ivgeni.
Hi Ivgeni,
I have answered the same question on your new thread. Please help us to close this thread.
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/362470/1273452.aspx#1273452
Thanks,