Hi
we are testing in connection between c6670's AIF2 and Xilinx CPRI IP core.
(Xilinx Fpga is set to a slave and c6670 is considered as a master.)
at first try, link(frame sync) status was abnormal in c6670. (maintains "unsync" status)
but we got "FRAMESYNC" status by connecting FPGA's recoverd clock(30.74MHz) to DSP(6670)'s PHYSYNC pin and RADSYNC pin.
here are questions.
1. Shoud PHYSYNC & RADSYNC pin requisitely be connected with FPGA??
Aren't AIF2 able to work properly with just only AIF2 differential Tx/Rx connection without any other connection with the opposite device.(like 6670's PHYSYNC pin)?
2. generally, What is a typical shape of AIF2's physical connection with counterpart device?
3. Can you give me any hints about software configurations as a 2nd question's answer, if possible.
thanks in advance.
Lee