We are using the UPP bus on the C6655 interfaced to an FPGA. We have set channel B up in transmit mode and set bit 28 of UPICR to 1 and bit 17 to 0. This should program the Enable signal to be active high and change on the falling edge of the clock. We are seeing the Enable signal go high 4 ns after the falling edge of the clock but the Enable signal goes low approximately 8 ns after the rising edge of clock. We are running at 18.75 MHz. I have attached logic analyzer screen shots of the falling edge of the Enable signal. Do you know why the Enable signal is going low off the rising edge of the clock?