Hello everyone,
Target is C6678.
From the SRIO UG for the LSU_REG4 SUP_GINT bit it says :
"Suppress good interrupt.
If “interrupt request” is set, and this bit is
- ‘0’ Interrupt will be generated on good completion as well
-‘1’ interrupt will be suppressed on a good completion"
My question is :
when interrupt request is not set, sup_gint should be set to 0 or 1 ?
I want to make sure to receive the 'bad lsu0 interrupts' in all cases.
Thank you,
Clement