Hi
Can someone please help me with this error message I get when I try to run my code?
A0=0x1 A1=0xc026880
A2=0x1 A3=0x8091c0
A4=0x1 A5=0x1
A6=0x0 A7=0x1800080
A8=0x0 A9=0x8077ac
A10=0x5 A11=0x3
A12=0x0 A13=0x8077f0
A14=0xc0269e0 A15=0x0
A16=0x803f9c A17=0x0
A18=0x803f6c A19=0x20
A20=0x0 A21=0x0
A22=0x3a8eca58 A23=0x4468202
A24=0xf4601905 A25=0x1d70ca14
A26=0xeb598483 A27=0xc4b11ebf
A28=0xc084908 A29=0x23
A30=0x803f20 A31=0x0
B0=0x0 B1=0x0
B2=0x0 B3=0x0
B4=0x98 B5=0x1
B6=0x8078b0 B7=0xa
B8=0xc085d20 B9=0x0
B10=0x0 B11=0x0
B12=0x18000a0 B13=0xc02e680
B14=0x804000 B15=0x803dd8
B16=0xc036e90 B17=0xc036e58
B18=0x80000 B19=0xf00
B20=0x40 B21=0x0
B22=0xd B23=0x0
B24=0x8077f4 B25=0x4
B26=0xc08491c B27=0x620
B28=0x1 B29=0x1b60
B30=0x807350 B31=0x1f
NTSR=0x1020f
ITSR=0xd
IRP=0xc034338
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x0
EFR=0x2 NRP=0x0
Internal exception: IERR=0x11
Instruction fetch exception
Resource conflict exception
ti.sysbios.family.c64p.Exception: line 256: E_exceptionMax: pc = 0x00000000, sp = 0x00803dd8.
xdc.runtime.Error.raise: terminating execution
I have tried to increase the stack size to 16K
For information I run the code on a C6655 where there is no DDR3 RAM, which means that I only use MSMCSRAM and L2SRAM, I have attatched the mapfile for reference.
It is not always both exeptions htat comes - sometimes it is only the Instruction fetch, but I have no idea why.
0488.ConvFW_ct440_test.map.txt
Thanks
Jens Biltoft