Hello,
We have been producing a product with the TMS320C6672 for a little over a year, and have been happy with it, but we had an application where we needed to make use of the 1.25GHz version (TMS320C6672ACYP25). We recently did a run of boards with the new part, and started by running out existing software, which runs at 1GHz.
With the same code, our current consumption doubled, and the part shuts down due to the excess heat.
We haven't done a build since earlier this year. Our guess is that maybe a change was made to the die, and our code might need to change as well, but we aren't sure. Was there a change to the part recently? Or is the 1.25GHz a totally different die?
Based on the power calculator, we would expect a rise in current with increased speed, but didn't expect to see a jump just moving to the 1.25GHz part. Is there something we are missing?
Thank you