Hi,
I have a question about SALLD which is for Keystone Device.
After creating CCS project using saProjectCreate.bat, I check the Properties of project from CCS.
In Properties -> General -> "Main" tab, Device Variant was set to "Generic C64x+ Device
and -mv64x+ was set in C6000 Compiler option.
The device is Keystone so that target is C66x device.
Is there any reason why "Generic C64x+ Device" and "-mv64x+" are used?
Is there any problem if I change this properties to "Generic C66x Device" and "-mv6600"?
I'm going to integrate this SA project to my own project.
In my project, "Generic C66x Device" and "-mv6600" are used.
best regards,
g.f.