Hello Support Team,
After configuring Linux for 66ak2h12 to only use 2 ARM cores, I would like to connect the debugger to any of the other two cores. I get the following response:
Error connecting to the target:
(Error -6503) PRSC module failed to write to a router register.
(Emulation package 5.1.507.0)
We can connect to the DPS:s and debug them, so the debugger is at least connected in the correct way.
I would like to connect to the ARM, download some code to RAM and execute it. Is this possible to do via the debugger? If so, any idea what I'm doing wrong?
Thank You,
/Peter Lööf