Hello.
I currently have an application that works well when I program the application over the JTAG cable from a Windows PC. I would like to program this application to the nand memory on the EVM.
I'm using the C6657 EVM that you can purchase from TI's store: http://www.ti.com/tool/tmdsevm6657
My current test is that the first thing my application does is turn off 4 the 4 LEDs that are on the board. However, it never gets to this point with any of the attempts that I've done to try and program the nand.
Is there a document available that documents the procedure to turn a application.out file from CCSv5 to whatever format the nand needs, and then whatever is needed to program that image to the DSP, and then what DIP switches should be used to boot that image.
I've attempted to follow the instructions in /opt/ti/mcsdk_2_01_02_06/tools/writer/nand but I have had no success.
Thanks,
Bill Lynch