Hi,
First of all, a short description of my system:
I working on a Keystone II EVM board (XTCIEVMK2X) rev 1.1 with the MCSDK 3.1.0.3
I have installed the CCS v5.5.0.77 with the keystone2 emupack 1.1.
My workstation is an Ubuntu 14.04.
In no boot mode, when I try to connect to the 8 DSP cores simultaneously,
CCS crash when connecting to the last core, no matter which core Id I connected last.
My ccxml files is configured with:
- Connection : TI XDS2xx USB Emulator
- Board: TCI6636K2H
- Gel Files: I have tried none and xtcievmk2x.gel (on dsp core only) but it behaves the same.
CCS crashing, I have used a screenshot to see the error :
"Error connecting the target: (Error -2172 @ 0xD) Unable to communicate with the emulator. {...} (Emulation package 5.1.232.0)"
Do I have configured well my ccxml file ? Is it a known issue ?
BR,
Julien Heulot