Hello,
I import post_evmc6678l project from mcsdk_2_01_02_06\tools\post\evmc6678l
Because the default properties did not generate .bin file, I added "${CCE_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin.bat" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/ofd6x.exe" "${CG_TOOL_ROOT}/bin/hex6x.exe" "${CCE_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin.exe" to Post-build steps.
I checked that bin file was generated from out file
However, the bin file is too big to download. The file size is 82KB.
I did not change anything in source, just added post-build steps.
Why is the size of bin file bigger than 64KB and how can I reduce it?
CCS version I am using is 6.0.1.00040,
And I am using mcsdk_2_01_02_06