I'm using a custom board with 2 C6678DSP and a SRIO Switch.
This board is connected to another 8 Board with a SRIO Bus
For flexibility reason i want to remap the address used by SRIO, for example dedicate al the 4GB address space to the 4GB DDR3 space or create different memory buffers in the L2 of the cores and in the Shared Memory
So i want to use the SMS_MPAX and the SES_MPAX registers for the PrivID 9 (SRIO) and remap the incoming address.
The Doubt is: SMS_MPAX is for Shared Memory and SES_MPAX is for external DDR3 memory.
So, it's impossible to remap the incoming address to the Local L2 memory of the 8 cores? Or is still possible?