Hi all,
The LCD displayed "Main Power Failure" on K2HEVM. My rescue steps as follows.
1. Update BMC to latest version 1.0.2.5
Here was my console log.
0245.BMC VERSION 1.0.2.5.log
=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2014.09.18 17:38:28 =~=~=~=~=~=~=~=~=~=~=~= [2J [100BBMC> BMC VERSION 1.0.2.5 BUILT May 14 2013 11:46:18 --------------------- BMC> [00:00:00] BMC> BMC Init BMC> Begin BMC> [00:00:00] BMC> BMC Version BMC> 1.0.2.5BMC> BMC> [00:00:00] BMC> XTCIEVMK2X BMC> [00:00:00] BMC> 3.1 BMC> [00:00:00] BMC> S/N: 94621 BMC> [00:00:00] BMC> BMC Init BMC> Complete BMC> [00:00:00] BMC> Main PWR Start BMC> Begin BMC> [00:00:00] BMC> EVM setup has encountered the following error: The signal MAIN_POWER_GOOD has failed to assert BMC> [00:00:00] BMC> Main PWR Stop BMC> Begin BMC> [00:00:00] BMC> Main PWR Stop BMC> Complete BMC> [00:00:01] BMC> HWDBG is set to ON, evm setup will now halt. BMC> [00:00:01] BMC> To alter this behavior, please use the hwdbg command. BMC>ver [00:00:03] BMC>ver BMC> [00:00:03] BMC> Executing command "ver" BMC> [00:00:03] BMC> BMC> [00:00:03] BMC> BMC Version EVM Type EVM Superset EVM Subset EVM Version EVM S/N UCD Ver BMC> [00:00:03] BMC> 1.0.2.5 0.0.0.1 K2KH-EVM XTCIEVMK2X 3.1 94621 BMC> [00:00:03] BMC> BMC>