Hello
I have a TMDSEVM6670LE board and I have to use big endian. so I want to change project big endian.
so I start to change POST project first.
I build POST project on big endian.
And board power up, I connect to board mezzanine Debugger,
And I run CCS mode. POST is good working.
Next,I want to flash POST program in EEPROM. but not boot. I think.
This is my process.
1. I build POST program on big endian. and I check post_evm6670l.out
2. post_i2crom.bin doesn't made. so I use shell script, name is post_romparse.sh
3. I edit post_romparse.sh (CGT_INSTALL_DIR, ENDIAN) and I check post_i2crom.bin file, including modified date.
4. I copy post_i2crom.bin file into mcsdk/tools/writer/eerprom/evmc6670l/bin
5. I modify DIP switch no boot mode.
6. I modify eepromwriter_input.txt (file_name = post_i2crom.bin, bus_addr = 0x50, start_addr = 0, swap_data = 0)
7. I run CCS with eepromwriter_evm6670.out (eepromwriter_evm6670.out is built on big endian)
8. I follow README.txt file. and I see a succeful message.
9. Turn off my board, and I modify DIP switch I2C boot mode with address 0x50.
10. Turn on my board. and I check LED.
unfortunately, All LED are ON. Not changed.
what I miss it?
thank you
regards