Hi:
I just follow the Ti's steps. But only one core can bring up successfully.
anything wrong?
Kernel log.
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Linux version 3.10.10-svn148 (william@ubuntu) (gcc version 4.9.1 20140710 (prerelease) (crosstool-NG linaro-1.13.1-4.9-2014.07 - Linaro GCC 4.9-2014.07) ) #5 SMP PREEMPT Wed Oct 1 18:36:51 CST 2014
[ 0.000000] CPU: ARMv7 Processor [412fc0f4] revision 4 (ARMv7), cr=30c7387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine: KeyStone2, model: nsn,fzm
[ 0.000000] bootconsole [earlycon0] enabled
[ 0.000000] switching to high address space at 0x840000000
[ 0.000000] INITRD: 0x802000000+0x00900000 is not a memory region - disabling initrd
[ 0.000000] cma: CMA: reserved 20 MiB at 6e400000
[ 0.000000] Memory policy: ECC disabled, Data cache writealloc
[ 0.000000] DT missing boot CPU MPIDR[23:0], fall back to default cpu_logical_map
[ 0.000000] PERCPU: Embedded 8 pages/cpu @c3164000 s12160 r8192 d12416 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 752144
[ 0.000000] Kernel command line: console=ttyS0,115200n8 rootwait=1 earlyprintk rdinit=/sbin/init rw root=/dev/ram0 initrd=0x802000000,9M
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 2944MB = 2944MB total
[ 0.000000] Memory: 2942572k/2942572k available, 72084k reserved, 2236416K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef800000 ( 760 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc06e2fa4 (7020 kB)
[ 0.000000] .init : 0xc06e3000 - 0xc198cf80 (19112 kB)
[ 0.000000] .data : 0xc198e000 - 0xc19d0fd8 ( 268 kB)
[ 0.000000] .bss : 0xc19d0fd8 - 0xc1a3a784 ( 422 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ipc irq: irqchip registered, range 512-539
[ 0.000000] main_pll_clk rate is 0, postdiv = 2, mult = 19,prediv = 0
[ 0.000000] main_pll_clk rate is 1228800000, postdiv = 2, mult = 19,prediv = 0
[ 0.000000] Architected local timer running at 204.80MHz (phys).
[ 0.000000] Switching to timer-based delay loop
[ 0.000000] sched_clock: ARM arch timer >56 bits at 204800kHz, resolution 4ns
[ 0.000000] keystone timer clock @204800000 MHz
[ 0.000000] sched_clock: 32 bits at 100 Hz, resolution 10000000ns, wraps every 4294967286ms
[ 0.000000] Console: colour dummy device 80x30
[ 72.611418] Calibrating delay loop (skipped), value calculated using timer frequency.. 409.60 BogoMIPS (lpj=2048000)
[ 72.620155] pid_max: default: 32768 minimum: 301
[ 72.624103] Mount-cache hash table entries: 512
[ 72.635834] Initializing cgroup subsys net_cls
[ 72.639600] CPU: Testing write buffer coherency: ok
[ 72.643810] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 72.648545] Setting up static identity map for 0xc0526b40 - 0xc0526b74
[ 73.533651] CPU1: failed to come online
[ 74.369569] CPU2: failed to come online
[ 75.205487] CPU3: failed to come online
[ 75.208720] Brought up 1 CPUs
[ 75.211228] SMP: Total of 1 processors activated (409.60 BogoMIPS).
[ 75.216458] CPU: All CPU(s) started in SVC mode.
[ 75.220755] devtmpfs: initialized
[ 75.235067] NET: Registered protocol family 16
[ 75.239537] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 75.248735] gpio-keystone 260bf00.gpio: Runtime PM disabled, clock forced on.
[ 75.254714] gpio-keystone 260bf00.gpio: Invalid mem resource
[ 75.259445] gpio-keystone: probe of 260bf00.gpio failed with error -22
[ 75.269550] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 75.276226] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 75.292281] bio: create slab <bio-0> at 0
[ 75.295978] keystone-pcie: keystone_pcie_rc_init - start
[ 75.300464] keystone2_pcie_serdes_setup
[ 75.305379] keystone2_pcie_serdes_setup done, en_link_train = 1
[ 75.310342] keystone-pcie: MEM 0x0000000050000000..0x000000005fffffff -> 0x0000000050000000
[ 75.317363] keystone-pcie: IO 0x0000000024000000..0x0000000024003fff -> 0x0000000000000000
[ 75.324254] keystone-pcie: pcie - number of legacy irqs = 4
[ 75.328956] keystone-pcie: pcie - number of MSI host irqs = 8, msi_irqs = 32
[ 75.419098] keystone-pcie: Doing PCI Setup...Done
[ 75.423035] keystone-pcie: Starting PCI scan...
[ 75.426908] PCI host bridge to bus 0000:00
[ 75.430376] pci_bus 0000:00: root bus resource [mem 0x50000000-0x5fffffff]
[ 75.436102] pci_bus 0000:00: root bus resource [io 0x0000-0x3fff]