HI, experts:
hardware platform:66AK2H12
software paltform:CCS5.5
I am developing 66AK2H12 at present, and I had developed 6678 for sever years, I think the difference between 66AK2H12 and 6678 is that 66AK2H12 has A15 need to develop than 6678, but the developing of ARM A15 is difficulty for us, so I have some questiones to consult you:
1. Is the developing of ARM A15 must on the linux host,? from the wiki, I see this sentence:
- Toolchain: Must be installed on Linux Host. Ubuntu 12.04 recommended.
2. DO ARM A15 must run on linux system?
3. If ARM A15 rum linux, dsp core run SYS/BIOS, how do they communite? can you give me a suggests.
Best Regards
Gavin