This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Communication between 2 TMDSEVM6678L

Hello Sir,


I have two EVMs TMDSEVM6678L and I am trying to fix a connection via port 1 RJ45 using the PA_emacExample. I want something very very simple point to point connection. My objective is to pass some packets from the one EVM to other. I understand how the module works and i can use both of EVMs to send packets to a PC capturing them with wireshark. However i can not send packets between the EVMS. (but i think that the one EVM update the ALE switch of the other)

What kind of configurations I have to make? I can use the same IPs (10 11 12 ..) or I must change?

In switch ALE?

I want to deactivate the PA filtering. So I entered zero in all MAC and IP values.


Can I deactivate The IP protocol somehow considering a point to point connection?

I have to configure the PHYs? (I have the source codes provided by this forum) or is not needed?

Attention : I dont want to make a functional application. I only want to send some packets with the easiest way for validation reasons


Cordialement

Panagiotis

  • Hi,

    There is no direct test code to check your scenario like to communicate between two EVMs. But some of the discussion held in the below E2E post for your test case.

    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/202083.aspx
    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/202083/719489.aspx#719489
    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/196299/700615.aspx#700615

    Hope, this will help you.