HI,
I am using the C6670 DSP, for GSM baseband processing.
For the Layer 1 and Layer 2 interface we are using the ethernet packets "IPv4".
The NETCP - PA module takes care for the L2,L3,L4 header decoding and the corresponding PDSP firmware is provided by TI.
Currently it is supporting the IPv4, can it support IPv6 ? If yes , can you share a sample code/example using the IPv6 packets.
Regards,
Manav