I recently succeeded in getting an EVMK2H board to boot via TFTP/NFS and have been able to connect to it via SSH. I was trying to install the toolkit on the EVM and, as instructed by the user guide, rebooted the board (via "reboot" shell command).
From that point on, the system won't boot anymore. These are the last lines printed by the kernel:
[ 19.588839] IP-Config: Complete: [ 19.591989] device=eth0, hwaddr=b4:99:4c:9b:d0:d2, ipaddr=129.132.157.78, mask=255.255.255.0, gw=129.132.157.1 [ 19.602186] host=keystone-board, domain=, nis-domain=(none) [ 19.608045] bootserver=129.132.4.35, rootserver=129.132.4.35, rootpath= [ 19.614763] nameserver0=129.132.98.12, nameserver1=129.132.250.2 [ 19.656873] VFS: Mounted root (nfs filesystem) on device 0:11. [ 19.662751] Freeing unused kernel memory: 328K (c0700000 - c0752000) [ 30.111110] System halted.
These are the kernel parameters:
[ 0.000000] Kernel command line: console=ttyS0,115200n8 rootwait=1 verbose debug ignore_loglevel rootfstype=nfs root=/dev/nfs rw nfsroot=129.132.4.35:/scratch/cunokl/keystone-blank,v3,tcp,rsize=4096,wsize=4096 mtdparts=davinci_nand.0:1024k(bootloader)ro,512k(params)ro,129536k(ubifs) nfsrootdebug mem=512M ip=129.132.157.78:129.132.4.35:129.132.157.1:255.255.255.0:keystone-board:eth0:off:129.132.98.12:129.132.250.2
I also tried unpackaging a new root filesystem (tisdk-rootfs.tar.gz) and booting using that one, but I get exactly the same result.
Any ideas?