I am trying to run the hyperlnk_exampleProject provided by the MCSDK. However, when I try to build the project I get an error of incompatible XDCTools version. However, the version which the builder complains about should be installed or supported by the later 3.30.3.47 version which is also installed.
If I look in the "Build Settings" -> General -> RTCS: all the MCSDK tools which should be provided by the MCSDK-package is noted by a red cross indicating that the package is either not installed or not campatible version.
I have tryed to reinstall both CCS 6.0 and MCSDK, but it didn't make things better.
Can you help, to what I am dooing wrong?