Hello all,
CCS5.5 crashed whenever I add a memory read to address 0x60000000.
I was developing a pcie code and added the following to my WORKING PROJECT
volatile UInt32 *pcieDataBase = (UInt32 *)0x60000000;
and inside my code, I do:
for (k = 0; k < 2*3072; k++)
algInputBuff[k] = *((volatile uint32_t *)pcieDataBase + k);
When I use CCS to load and run the project, it crashed and I get the errors shown in the attached document. WHEN I load the project into NOR Flash and boot from I2C, EVERYTHING WORKS FINE!
Note: I am committing all the pcie code to eliminate pcie configuration issues.
How can I fix this issue and is it related to CCS debug only?
Regards,
Murad