Hello,
I have a 66AK2E05 CPU. I want to boot the processor via ethernet with minimum boot pin select, but it doesn't work.
The PA clk source is NETCPCLK (156,25MHz) select via NETCPCLKSEL = 1. I think the Ref Clock coming from the SGMII clock (156,25MHz). The core clock is 156,25MHz.
When the system is configured with non minimum boot pin select and the other pins have the default values for ethernet minimum boot pin select it works. I test the minimum boot pin select for uart and spi and it works.
Can anyone help me?